Android build for MCIMX6Q-SDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android build for MCIMX6Q-SDB

1,264件の閲覧回数
Gandalf-kern
Contributor IV

Which of these two builds work correctly on the MCIMX6Q-SDB, or which is the correct BSP?

sabreauto_6q i.MX 6Quad Auto Infotainment

sabresd_6dq i.MX 6DualQuad SABRE Board and SABRE Platform

These are taken from the android_L5.0.0_1.0.0-ga_... published/Android User's Guide.

0 件の賞賛
返信
1 返信

1,182件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

MCIMX6Q-SDB relates to sabresd_6dq i.MX 6DualQuad SABRE Board and SABRE Platform.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------