Android R13.4.1.02 Release

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android R13.4.1.02 Release

2,909 Views
EnriqueOchoaVaz
Contributor V

Hi All,

The new  Android R13.4.1.02 release is now available on the http://www.freescale.com/site.

·         Files available

#

Name

Description

Files

1

IMX6_R13.4.1.02_ANDROID_PATCH

Android   13.4.1.02 patch release supports to run i.MX 6Solo emulation on i.MX   6DualLite SABRE-SD platform. Patch based on Android 13.4.1 BSP. Includes   source code, demo image and MFG tool

Link

·         Target HW boards

o   i. MX6DL  Sabre SDP board

·         Known issues

o   For known issues and limitations please consult the release notes

Labels (2)
0 Kudos
Reply
2 Replies

2,086 Views
bikash
Contributor II

Hii,

  I am trying to run imx6 sabre sd dual-lite board in solo mode. I applied the u-boot patches in bootable/bootloader/u-boot of android r13.4.1 release. But it's not booting. The log we are getting is as follow:

U-Boot 2009.08-00635-g5a8341b (Feb 08 2013 - 14:37:50)

CPU: Freescale i.MX6 family TO1.1 at 792 MHz

Temperature:   can't get valid data!

mx6q pll1: 792MHz

mx6q pll2: 528MHz

mx6q pll3: 480MHz

mx6q pll8: 50MHz

ipg clock     : 66000000Hz

ipg per clock : 66000000Hz

uart clock    : 80000000Hz

cspi clock    : 60000000Hz

ahb clock     : 132000000Hz

axi clock   : 198000000Hz

emi_slow clock: 22000000Hz

ddr clock     : 396000000Hz

usdhc1 clock  : 198000000Hz

usdhc2 clock  : 198000000Hz

usdhc3 clock  : 198000000Hz

usdhc4 clock  : 198000000Hz

nfc clock     : 24000000Hz

Board: i.MX6DL/Solo-SABRESD: unknown-board Board: 0x61011 [POR ]

Boot Device: SD

I2C:   ready

DRAM:  512 MB

MMC:   FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3


0 Kudos
Reply

2,086 Views
EnriqueOchoaVaz
Contributor V

Hi,

Can you enter this question as a new question on the community? That will help us to track the solution because this publication was not entered as a question.

Regards

0 Kudos
Reply