Android Porting on SABRE-SD IMX6DL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android Porting on SABRE-SD IMX6DL

4,308 次查看
kapilkumar
Contributor III

Hi Friends

I am trying to bring up my board (MCIMX6DL-SDP) using Android jb4.3_1.1.0  BSP. Building of all the required images (boot.img , system.img , recovery.img , u-boot-6dl.bin ) had been done.

Now, when i am trying to do booting up of  the board using sd card (8GB), android logo is flashing and stuck over there. I used MFGToolsV2 for downloading all the images into the card.

Can anyone help me kindly to find out the solution for this problems??

I am also attaching here hyperterminal log.

Thank You

Kapil Kumar.

标签 (2)
0 项奖励
回复
1 回复

3,427 次查看
art
NXP Employee
NXP Employee

The better way is to immediately migrate to the latest Lollipop 5.1.1_2.1.0 BSP, available for download on the NXP web site (check the "Board Support Packages" section):

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

since no further JellyBean support is planned.

First, try the pre-built images or even pre-built MFGtool package (check the "Programmers (Flash, etc.)" section). Also, refer to attached document for the information on how to prepare BSP and SD card.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复