Android Oreo 8.0: Use two displays with different resolution

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android Oreo 8.0: Use two displays with different resolution

1,806 Views
jdepedro
Contributor IV

I am using the default images on the i.MX6 reference board and I see that when using HDMI + LVDS display, Android works in mirror mode showing the same content in both displays, rescaling it if needed.

How can I configure Android so that different resolutions are used? (The HDMI negociated resolution for HDMI, and the LVDS native resolution for the LVDS display)

0 Kudos
Reply
1 Reply

1,688 Views
joanxie
NXP TechSupport
NXP TechSupport

you can boot up dual display successfully, but couldn't show the different resolution, right? pls refer to the topic as below:

https://community.nxp.com/thread/384600 

0 Kudos
Reply