Android Nought incoming/outgoing call error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android Nought incoming/outgoing call error

1,960 Views
vinothkumars
Senior Contributor IV

Dear NXP,

 

   I am working on Toradex apalis imx6q with Android Nougat. we got the issue, once we disconnect outgoing call, incoming call UI is coming abruptly.

Steps::
1. connect the phone(android or iphone) to our custom board.
2. Make the outgoing call.
3. After accepting the call , disconnect the call.

Observation::

Android::
   incoming call UI is coming abruptly and it is remain same for long time.

Iphone::
   incoming call UI is coming abruptly and suddenly it is refershing.

What could be the issue. and which side these issue came either BSP or Application.

Regards,

VinothS

Regards,
Vinothkumar Sekar
Labels (2)
0 Kudos
Reply
2 Replies

1,877 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, the GSM module is not currently supported in our BSP, I recommend you to go with Toradex, probably they could help you.

Best regards,

Diego.

0 Kudos
Reply

1,877 Views
vinothkumars
Senior Contributor IV

Hi Diego,

Thank you for your reply. This is the problem from the Android application side, and this one fixed by Android Application developer. 

So, we close this thread now.

Thanks & Regards,

VinothS

Regards,
Vinothkumar Sekar
0 Kudos
Reply