Android Nought incoming/outgoing call error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android Nought incoming/outgoing call error

1,971件の閲覧回数
vinothkumars
Senior Contributor IV

Dear NXP,

 

   I am working on Toradex apalis imx6q with Android Nougat. we got the issue, once we disconnect outgoing call, incoming call UI is coming abruptly.

Steps::
1. connect the phone(android or iphone) to our custom board.
2. Make the outgoing call.
3. After accepting the call , disconnect the call.

Observation::

Android::
   incoming call UI is coming abruptly and it is remain same for long time.

Iphone::
   incoming call UI is coming abruptly and suddenly it is refershing.

What could be the issue. and which side these issue came either BSP or Application.

Regards,

VinothS

Regards,
Vinothkumar Sekar
ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,888件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, the GSM module is not currently supported in our BSP, I recommend you to go with Toradex, probably they could help you.

Best regards,

Diego.

0 件の賞賛
返信

1,888件の閲覧回数
vinothkumars
Senior Contributor IV

Hi Diego,

Thank you for your reply. This is the problem from the Android application side, and this one fixed by Android Application developer. 

So, we close this thread now.

Thanks & Regards,

VinothS

Regards,
Vinothkumar Sekar
0 件の賞賛
返信