Android Image on USB Flash for i.MX6 Android 6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android Image on USB Flash for i.MX6 Android 6

1,753件の閲覧回数
cxbere
Contributor I

Hello Everyone,

I have a custom board which is designed based i.MX6dl. In my system, first u-boot is loaded from a SPI Flash and then all other Ramdisk, Android System images are loaded eMMC or SD card. It is working very well now. But I need to load Ramdisk, System Image from USB stick.

I mean that, I want to use flash memory instead of SD card or eMMC. I have searched flastboot, but I can't use a PC from OTG, my device is working standalone and using a PC is very hard to update image in industrial environment.

Best Regards,

Ercüment TÜRK

タグ(4)
0 件の賞賛
返信
1 返信

1,530件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ercüment

unfortunately such configuration is not provided (not supported) by nxp

in its android releases described on official i.MX software link

i.MX Software|NXP 

one can apply to Professional Services for developing that custom solution

NXP Professional Services|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信