Android 9 USB pendrive not detected in system level

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android 9 USB pendrive not detected in system level

2,256 Views
aravinthkumarja
Senior Contributor II

Hi All,

I'm using Android 9 in imx6 board. 

I'm using USB H1 and defined in fstab.freescale. 

/devices/soc0/soc/2100000.aips-bus/2184200.usb/ci_hdrc.1* auto auto defaults voldmanaged=usb:auto

 

After boot If I insert pendrive its detected under /dev/block/sda1 

But it not showing inside  /dev/block/vold/ .   

So its not auto mounting also.

 

Can you please help to fix it.

 

Regards,

Aravinth

0 Kudos
Reply
2 Replies

2,221 Views
Aravinthkumar
Contributor III

Hi,

We have fixed the issue.

 

Thank you.

0 Kudos
Reply

2,233 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Could you please share which i.MX6 are you using?
is it a custom board or an NXP board?
If possible, could you share the full logs?

Also, please remember that if you're using i.MX6 SABRE Board the only USB supported should be the OTG one, and it is already defined at fstab.freescale:

/devices/soc0/soc/2100000.aips-bus/2184000.usb/ci_hdrc.0*  auto auto defaults voldmanaged=usb:auto

Best regards,
Aldo.

0 Kudos
Reply