Android 9 USB pendrive not detected in system level

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android 9 USB pendrive not detected in system level

2,268 次查看
aravinthkumarja
Senior Contributor II

Hi All,

I'm using Android 9 in imx6 board. 

I'm using USB H1 and defined in fstab.freescale. 

/devices/soc0/soc/2100000.aips-bus/2184200.usb/ci_hdrc.1* auto auto defaults voldmanaged=usb:auto

 

After boot If I insert pendrive its detected under /dev/block/sda1 

But it not showing inside  /dev/block/vold/ .   

So its not auto mounting also.

 

Can you please help to fix it.

 

Regards,

Aravinth

0 项奖励
回复
2 回复数

2,233 次查看
Aravinthkumar
Contributor III

Hi,

We have fixed the issue.

 

Thank you.

0 项奖励
回复

2,245 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Could you please share which i.MX6 are you using?
is it a custom board or an NXP board?
If possible, could you share the full logs?

Also, please remember that if you're using i.MX6 SABRE Board the only USB supported should be the OTG one, and it is already defined at fstab.freescale:

/devices/soc0/soc/2100000.aips-bus/2184000.usb/ci_hdrc.0*  auto auto defaults voldmanaged=usb:auto

Best regards,
Aldo.

0 项奖励
回复