AnTuTu doesn't work on MCIMX7SABRE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AnTuTu doesn't work on MCIMX7SABRE

2,193 Views
ko-hey
Senior Contributor II

Hi all

 

I want to use AnTuTu for comparing the i.MX7 CPU performance. 

However, it doesn't work and got two following error.

 

Does someone use AuTuTu with MCIMX7SABRE ?

Could someone give me advise to resolve this issue ?

 

Here is my environment and I attached the log when I click those icons.

------------------------------------------

Android: N7.1.1 (Demo image download from NXP)
AnTuTu Benchmark: 6.3.3
Board: MCIMX7SABRE
Display: LCD8000-43T 

------------------------------------------

 

 

 

1. Error message when I click AnTuTu icon

188645_188645.JPGIMG_0319.JPG

 

2. Error message when I click "Open app again" message

188646_188646.JPGIMG_0320.JPG

 

Ko-hey

Original Attachment has been moved to: error_message-AnTuTu-Benchmark-has-stopped.txt.zip

Original Attachment has been moved to: error_message-AnTuTu-Benchmark-keeps-stopping.txt.zip

0 Kudos
Reply
4 Replies

1,973 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Thank you for writing.

Have you tried to ask directly to the AnTuTu developers?

Because, unfortunately, we do not give support to Android applications.

Best Regards,

Diego

0 Kudos
Reply

1,973 Views
ko-hey
Senior Contributor II

Hi diegoadrian‌

Thank you for reply.

I've never asked to AnTuTu developers because I don't know the link.

Do you know ?

Add info:

I tried following thread but not work well.

https://community.nxp.com/thread/448760 

Ko-hey

0 Kudos
Reply

1,973 Views
diegoadrian
NXP Employee
NXP Employee

Probably in this email, they can help you.

[email protected]

Regarding the selinux authority problem, during the booting process, before the kernel start up, you need to press any key of your keyboard, after that, you can change the "bootargs". The "bootargs" can vary depending of your setup.

This is an example of how to boot whit a single LDVS display:

U-Boot > setenv bootcmd boota mmc0

U-Boot > setenv bootargs console=ttymxc0,115200 init=/init androidboot.console=ttymxc0 consoleblank=0                androidboot.hardware=freescale androidboot.selinux=disabled

               androidboot.dm_verity=disabled

U-Boot > saveenv

I hope this can help you.

Best Regards,

Diego.

0 Kudos
Reply

1,973 Views
ko-hey
Senior Contributor II

Hi  diegoadrian‌

 

Thank you for the information of AnTuTu.

I'll ask them.

 

P.S.

I tried your suggested command but not work well.

 

Ko-hey

0 Kudos
Reply