Adeneo Embedded experts launch 2 dedicated blogs !

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adeneo Embedded experts launch 2 dedicated blogs !

2,099件の閲覧回数
witekio
Contributor III

Since january 2013, Adeneo Embedded launched 2 dedicated blogs. These blogs are both run by Adeneo Embedded Windows and Linux experts, multiple time MVP awarded.

The goal is to provide the windows and linux communities with specific up-to-date information as well as the latest announcements concerning these two companies.


Click here to visit our Windows dedicated blog


Click here to visit our Linux dedicated blog

Follow, comment and subscribe !

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,936件の閲覧回数
LeonardoSandova
Specialist I

Links have wrong names, the windows link points to the Linux and vice versa.

0 件の賞賛
返信

1,936件の閲覧回数
witekio
Contributor III

Thanks for the heads up Leonardo ! The problem is fixed now :smileyhappy:

0 件の賞賛
返信