Additional Chip Select lines for SPI interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Additional Chip Select lines for SPI interface

1,220 Views
harishs
Contributor I

Hi,

We are developing one of our product using CM-FX6  ( IMX6 Quad based COM form Compulab), is it possible to use available GPIO lines for additional Chip select lines for SPI interface required, the dedicated Chip select lines of SPI are used for some other interfaces in our design.

Regards,

Harish.S

Labels (1)
0 Kudos
Reply
1 Reply

1,144 Views
Yuri
NXP Employee
NXP Employee

Hello,

  It is possible to use available GPIO lines for additional Chip select lines for SPI interface.
But users should control these GPIO lins in software.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply