Adding patches to build uImage (AVB)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Adding patches to build uImage (AVB)

1,458 次查看
ajayvenkatakris
Contributor II

Hi I want to build a uImage for AVB. I have found the link with the required patches needed to build the uImage. But how and where should I add these patches for building the image? Should I add it in the local.conf file and if yes, how do I add it?

0 项奖励
回复
2 回复数

1,371 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ajay

please refer to yocto faq sect.2.2.2. Applying Patches

Yocto Project Linux Kernel Development Manual 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,371 次查看
ajayvenkatakris
Contributor II

Hi,

   There are many bbappend files available. I am building an fsl-image-gui for imx6dl sabre auto board. At exactly which bbappend file should I add the patch files?

0 项奖励
回复