Version is 4.4.2,I add the adv7180 device on IPU2 CSI1 ,but the board startup errors as shown in attachment.
modified board-imx6q_sabresd.c :
static void adv7180_pwdn(int pwdn)
{
if (pwdn)
gpio_set_value(SABRESD_CSI1_PWN, 1);
else
gpio_set_value(SABRESD_CSI1_PWN, 0);
}
static void mx6q_csi1_io_init(void)
{
if (cpu_is_mx6q())
mxc_iomux_v3_setup_multiple_pads(mx6q_sabresd_csi1_sensor_pads,
ARRAY_SIZE(mx6q_sabresd_csi1_sensor_pads));
else if (cpu_is_mx6dl())
mxc_iomux_v3_setup_multiple_pads(mx6dl_sabresd_csi1_sensor_pads,
ARRAY_SIZE(mx6dl_sabresd_csi1_sensor_pads));
if (cpu_is_mx6q())
mxc_iomux_set_gpr_register(1, 20, 1, 1);//by ruofeng
//mxc_iomux_set_gpr_register(1, 19, 1, 1);
else if (cpu_is_mx6dl())
//mxc_iomux_set_gpr_register(13, 0, 3, 4);
mxc_iomux_set_gpr_register(13, 3, 3, 4);
}
/*static struct fsl_mxc_tvin_platform_data adv7180_data = {
.dvddio_reg = NULL,
.dvdd_reg = NULL,
.avdd_reg = NULL,
.pvdd_reg = NULL,
.pwdn = adv7180_pwdn,
.reset = NULL,
.cvbs = true,
.io_init = mx6q_csi1_io_init,
};*/
static struct fsl_mxc_camera_platform_data adv7180_data = {
.mclk = 24000000,
.mclk_source = 0,
.csi = 1,
.io_init = mx6q_csi1_io_init,
.pwdn = adv7180_pwdn,
};
static struct i2c_board_info mxc_i2c2_board_info[] __initdata = {
.....
#ifdef MYDEBUG
{
I2C_BOARD_INFO("adv7180", 0x21),
.platform_data = (void *)&adv7180_data,
},
#endif
};
static struct fsl_mxc_capture_platform_data capture_data[] = {
{
.csi = 0,
.ipu = 0,
.mclk_source = 0,
.is_mipi = 0,
}, {
.csi = 1,
.ipu = 0,
.mclk_source = 0,
.is_mipi = 1,
},
#ifdef MYDEBUG
{
.csi = 1,
.ipu = 1,
.mclk_source = 0,
.is_mipi = 0,
},
#endif
};
static void __init mx6_sabresd_board_init(void)
{ ....
imx6q_add_v4l2_capture(0, &capture_data[0]);
imx6q_add_v4l2_capture(1, &capture_data[1]);
#ifdef MYDEBUG
imx6q_add_v4l2_capture(2, &capture_data[2]);
#endif
....
}
Where is my wrong Or what's the problem I overlooked? HELP!