Accelerometer Device Orientation Detection in vertical direction

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Accelerometer Device Orientation Detection in vertical direction

2,019件の閲覧回数
NeemaBhandary
Contributor I

Hi all,

I'm using application "AccSample" from following path for testing Accelerometer driver.

%_WINCEROOT%\platform\IMX313DS\SRC\TEST\ACCELEROMETER   

                                                        
        1.  Before enabling the rotation:  If the device is rotated both in horizontal and vertical direction then x,y & z co-ordinate values are getting updated.

         2. After rotation is enabled: If the platform is rotated in horizontal direction(flat) then orientation change is getting detected  and also the screen rotation                                                       is happening according to the device orientation. But Orientation change is not getting detected in the vertical direction i.e if                                                       the platform is kept vertical and rotated then screen rotation is not happening.

Please let me know the reason for this issue

Thank You

Neema


ラベル(2)
0 件の賞賛
返信
3 返答(返信)

1,768件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

Deactivated user can you help on this case?

0 件の賞賛
返信

1,768件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

0 件の賞賛
返信

1,768件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

No update from customer

0 件の賞賛
返信