Dear all,
Our customer runs Android4.4.2 on MX6Q-SABRE-SDB.
A SDXC card is mounted on Android4.4.2.
Howevwer, it is recognized as 0 GB.
And the contents of SDXC cannot be seen.
Does Android4.4.2_BSP of FSL support SDXC?
Best Regards,
Yuuki
A SDXC card is connected to a USB OTG port through a SD-USB adapter.
This SD-USB adapter corresponds to USB3.0.
It is recognized as 0 GB and the contents of SDXC cannot be seen.
If it is unmounted and then mounted, it is mounted correctly and the contents can be seen.
If the SD-USB adapter of USB2.0 correspondence is used, this problem will not occur.
Is this a problem of a SD-USB adapter?
Best Regards,
Yuuki
Hello Yuuki,
The 3.0 usb adapter could be the reason. Have you tried this adapter in the linux host?, can you check it and see what happens?