About splash screen for EPDC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About splash screen for EPDC

ソリューションへジャンプ
3,061件の閲覧回数
MasakiHayakawa
Contributor III

I try to test on i.MX6SLEVK.

BSP version  is fsl-yocto-L4.1.15_1.2.0-ga.

I want to create epdc_E060SCM_splash.bin, but I could not find the ihex2bin.py script.

Please provide it, because i.MX_Linux_Reference_Manual.pdf is indicated the following.

"2. Convert the ihex firmware file to a stripped-down binary using the script ihex2bin.py. Contact Freescale to acquire this script."

Best Regards

ラベル(2)
1 解決策
2,840件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
4 返答(返信)
2,840件の閲覧回数
MasakiHayakawa
Contributor III

Hi, igor

Thank you for your replay.

I try to contact.

0 件の賞賛
返信
2,840件の閲覧回数
MasakiHayakawa
Contributor III

Hi, igor

Thank you for your replay.

I looked for in NXP site, but I didn't know how to create service request.

Please tell me the way.

Best regards.

0 件の賞賛
返信
2,841件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

How to create service request :

https://community.freescale.com/docs/DOC-329745

~igor

2,840件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

please create service request for obtaining script.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信