About memtool support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About memtool support

2,238 次查看
matsumoto2
Contributor I

hello
I am using SC2310H to output data to MIPI of i.MX8MP, but the data does not reach the VB2 queue.
I would like to refer to the following register values to check whether the i.MX8MP can receive MIPI data.
32E4_0020: D-PHY status register (MIPI_CSI1_DPHY_STATUS)
32EC_007C: Gasket 0 ISI Pixel Count Register

But I'm trying to use memtool but the cpu hangs when I run the command.
Does memtool support i.MX8MP?
Please tell me.

0 项奖励
回复
4 回复数

2,218 次查看
joanxie
NXP TechSupport
NXP TechSupport

pls give me your memtool command, let me double check it

0 项奖励
回复

2,213 次查看
matsumoto2
Contributor I

"./memtool 0x32ec007c 1"
"./memtool 0x32e40020 1"

0 项奖励
回复

2,195 次查看
joanxie
NXP TechSupport
NXP TechSupport

when you read these registers, did you connect any camera?

0 项奖励
回复

2,186 次查看
matsumoto2
Contributor I

Connected to the camera of course.

I was able to confirm the target register by dumping it from the source code.
I was able to achieve my goal without using memtool.

0 项奖励
回复