About memtool support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About memtool support

2,241 Views
matsumoto2
Contributor I

hello
I am using SC2310H to output data to MIPI of i.MX8MP, but the data does not reach the VB2 queue.
I would like to refer to the following register values to check whether the i.MX8MP can receive MIPI data.
32E4_0020: D-PHY status register (MIPI_CSI1_DPHY_STATUS)
32EC_007C: Gasket 0 ISI Pixel Count Register

But I'm trying to use memtool but the cpu hangs when I run the command.
Does memtool support i.MX8MP?
Please tell me.

0 Kudos
Reply
4 Replies

2,221 Views
joanxie
NXP TechSupport
NXP TechSupport

pls give me your memtool command, let me double check it

0 Kudos
Reply

2,216 Views
matsumoto2
Contributor I

"./memtool 0x32ec007c 1"
"./memtool 0x32e40020 1"

0 Kudos
Reply

2,198 Views
joanxie
NXP TechSupport
NXP TechSupport

when you read these registers, did you connect any camera?

0 Kudos
Reply

2,189 Views
matsumoto2
Contributor I

Connected to the camera of course.

I was able to confirm the target register by dumping it from the source code.
I was able to achieve my goal without using memtool.

0 Kudos
Reply