About imx8mplus USB Certification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About imx8mplus USB Certification

3,435 Views
t2865k5
Contributor I

Dear NXP , 

HW : srg_imx8mplus (base on : imx8mplus ,and remove all type c USB HW)

(1) USB 3.0 -> USB 2.0 HUB -> output USB 2.0 signal .

(2) USB 3.0 -> USB 3.0 HUB -> out USB 3.0 signal .

How do I set up the USB register with a software ,and make the USB output parten all the time?
I need to use an instrument to test the USB 2.0 and USB 3.0 eye diagram.

 

 

t2865k5_0-1630057720409.png

 

0 Kudos
Reply
6 Replies

3,395 Views
t2865k5
Contributor I

Dear NXP ,

I have been waiting for your reply for a long time. Please reply to me as soon as possible.

0 Kudos
Reply

3,404 Views
t2865k5
Contributor I

Dear NXP ,

I want to output USB 3.0 partern for TYPE A .

About USB3.0 Host mode for TYPE A in page 187.

TX:

echo -1 > /sys/module/usbcore/parameters/autosuspend

echo "host" >> /sys/kernel/debug/usb/38100000.dwc3/mode

/unit_tests/memtool -32 0x38200430=0x0A010340

Test Results:
Instrument: No USB waveform measured

t2865k5_0-1630491004379.png

t2865k5_1-1630491031717.jpeg

 

 

 

0 Kudos
Reply

3,412 Views
t2865k5
Contributor I

Dear NXP ,

It explains USB2.0 test eye diagram mode for Type A in page 189.

I didn't find the USB3.0 test eye pattern for Type A. Can you tell me how to set ?

 

t2865k5_0-1630376459533.png

 

0 Kudos
Reply

3,422 Views
t2865k5
Contributor I

Dear NXP , 

Are imx8mplus and imx8 series related registers the same? 

I run command as follows:

memtool 0x20c9010 1

t2865k5_3-1630285931634.png

 

 

 

t2865k5_1-1630285693408.png

t2865k5_2-1630285718765.png

 

 

t2865k5_0-1630285544560.png

 

0 Kudos
Reply

3,419 Views
igorpadykov
NXP Employee
NXP Employee

seems i.MX8M Plus is the same as i.MX8MQ.

 

Best regards
igor

0 Kudos
Reply

3,429 Views
igorpadykov
NXP Employee
NXP Employee

Hi Albert

 

for usb certification one can look at AN12409

i.MX6/7/8 series USB Certification Guide

 

Best regards
igor

0 Kudos
Reply