hello:nxp friends?
I had some questions with imx8mm on android9 platform?
No1: use 《 mipi_dsi_dcs_write_buffer() 》 this interface write lcd parasm,while i found,it can not long write?
No2:while use uuu to download firmware to emmc on ubuntu18,the adb and fastboot is ok,while it return error with log is "FB:ucmd setenv fastboot_dev mmc"
Hi zhou
seems rm67191 driver have dcs long write for backlight brightness setting
function mipi_dsi_dcs_set_display_brightness() :
panel-raydium-rm67191.c\panel\drm\gpu\drivers - linux-imx - i.MX Linux kernel
>The imx8mm manual told us imx8mm is no longer supported framebuffer device,use drm instead?
please check Linux 5.4.3_1.0.0 Documentation for supported functionality.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
thanks igorpadykov
I had a question,when i call mipi_dsi_dcs_write_buffer() interface to write cmd data,it return 0 to us not erro code?
what happen?
while call mipi_dsi_dcs_read() interface to read lcd id,that return 1 byte correct value to us?
what happen? @igorpadykov
i was confused
thanks igorpadykov
I had a question,when i call mipi_dsi_dcs_write_buffer() interface to write cmd data,it return 0 to us not erro code?
what happen?
while call mipi_dsi_dcs_read() interface to read lcd id,that return 1 correct to us?
what happen? @igorpadykov
i was confused
By the way
No1:The imx8mm manual told us imx8mm is no longer supported framebuffer device,use drm instead?
so the log
[ 1.300514] Unable to create device for framebuffer 0; errno = -19
is ring way?
And sysfs in /dev or /class/sys/graphics are not created fbx device node