About i.MX6SL Register Settings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About i.MX6SL Register Settings

27,354件の閲覧回数
tony_l_cai
Contributor III

Hi,All

     Lot of Register Settings were involved in Reference Manual, but how will I Set these registers in codebase? Where are they,such as boot mode, BT_FUSE_SEL and so on.

     Thanks!

ラベル(2)
0 件の賞賛
返信
1 返信

27,034件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi tony

please check attached file with i.MX Tools overview, also

one can look at SDK, it shows OS -less programming

for i.MX6 processors

i.MX 6Series Platform SDK : Bare-metal SDK

please check how to build ltib

AN3875 Building a Linux Image and Downloading onto i.MX Processors Using a Virtual Machine

L3.0.35_4.1.0_ER_SOURCE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux BSP Source Code Files.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信