About eMMC Device locked in i.MX6 system.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About eMMC Device locked in i.MX6 system.

跳至解决方案
1,580 次查看
keitanagashima
Senior Contributor I

Dear All,

Hello. I have a question about internal boot ROM processing in i.MX6SDL.

Refer to the below device status register in eMMC card.

The "DEVICE_IS_LOCKED" bit had changed to "1" in eMMC card on my customer's board.

(eMMC Status : 1 = Device locked)

And, the board couldn't boot-up (No output to serial console).

eMMC_DEVICE_IS_LOCKED.png

[Question]

Does iROM in i.MX6SDL check this bit 25 and does stop access to eMMC?

Could you check the internal ROM code?

Best Regards,

Keita

标签 (4)
0 项奖励
回复
1 解答
1,037 次查看
igorpadykov
NXP Employee
NXP Employee

HI Keita

ROM does not check/change this bit. eMMC itself check it and

if locked, do not provide data to host. This is described in

sect.7.6.13 Card lock/unlock operation eMMC 4.41 specification

JESD84-A441.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,038 次查看
igorpadykov
NXP Employee
NXP Employee

HI Keita

ROM does not check/change this bit. eMMC itself check it and

if locked, do not provide data to host. This is described in

sect.7.6.13 Card lock/unlock operation eMMC 4.41 specification

JESD84-A441.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,037 次查看
keitanagashima
Senior Contributor I

Dear Igor,

Hello. Thank you very much!

Best Regards,

Keita

0 项奖励
回复