About difference in memory reading speed by the Android version for i.MX6 Quad.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About difference in memory reading speed by the Android version for i.MX6 Quad.

1,715件の閲覧回数
yuuki
Senior Contributor II

Dear all,

We run Android BSP on MX6Quad SABRE-SDB board.

We noticed that memory reading speed was different between Android4 .4.2 and Android4 .4.3.

<Measurement result>
* Android4.4.2
    eMMC Seq.Read=47.49MB/s,   SD Seq Read=22.69MB/s

* Android4.4.3
    eMMC Seq.Read=35.38MB/s,   SD Seq Read=17.92MB/s

Would you tell me the factor of the difference in this speed?

May I have any advice?

Best Regards,
Yuuki Murasato

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,610件の閲覧回数
b36401
NXP Employee
NXP Employee

Are you using the same way to measure the speed?

Please make sure that the board is running with the same clocks.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,610件の閲覧回数
yuuki
Senior Contributor II

Dear Victor-san,

I am sorry to delay.

Thank you for your support.

We measured by the same method.
The clock setting for eMMC/SD is the same, too.
The write speed is almost similar.

However, we seem that a performance of the reading speed may be inferior in Android4.4.3.

Are there any patches for eMMC/SD I/F in Android4.4.3?

Best Regards,
Yuuki

0 件の賞賛
返信