About create image from emmc using mfgtool/usb-otg

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About create image from emmc using mfgtool/usb-otg

1,655件の閲覧回数
cyndent
Contributor I

Hi

   I want to create a factory image from my board. The board only have emmc. I use mfgtool to burn image to emmc.And now i want to get image from /dev/mmcblk1p1.

    Now i'm writing the image to u-disk via usb-otg. But the system is running while i use 'dd' command to get image from /dev/mmcblk1p1.If some files changes while creating images, the images will go wrong.

   So can i use mfgtool get image from board? Or just mount emmc to pc as a disk via usb-otg?

ラベル(2)
0 件の賞賛
返信
1 返信

1,575件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mingyang

for emmc programming one can follow Linux Guide from nxp linux documentation:

https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_LINUX_DOCS&appType=license&location=null 

or tutorial from

Programming eMMC on i.MX6 - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信