About a file programing RGMII register for AndroidKK4.4.2 of MX6-SABRE-SD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About a file programing RGMII register for AndroidKK4.4.2 of MX6-SABRE-SD

1,927件の閲覧回数
yuuki
Senior Contributor II

Dear all,

Our customer changed registers of RGMII by using memtool.

memtool -32 0x20e0790=0x000c0000
memtool -32 0x20e0380=0x0001b020
memtool -32 0x20e0384=0x0001b020
memtool -32 0x20e038c=0x0001b020
memtool -32 0x20e0390=0x0001b020
memtool -32 0x20e0394=0x0001b020
memtool -32 0x20e0398=0x0001b020
memtool -32 0x20e0370=0x0001b020
memtool -32 0x20e0374=0x0001b020
memtool -32 0x20e0378=0x0001b020
memtool -32 0x20e037c=0x0001b020
memtool -32 0x20e036c=0x0001b020
memtool -32 0x20e0388=0x0001b020


They want to implement such registers setting to AndroidKK4.4.2.

Which file should these setting be programed by?
Would you teach this file name and the position?

Best Regards,
Yuuki

ラベル(1)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

1,636件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

He yuuki

driver locations one can look at attached file, also

I would suggest to look at link below

https://github.com/rabeeh/android-imx6-kitkat/blob/master/platform/external/linux-test.git/0400-ENGR...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,636件の閲覧回数
yuuki
Senior Contributor II

Dear igor-san,

Thank you for your support.

Our customer wants to set the Ethernet in U-Boot.

Probably, I think that it is set at the following.
bootable/bootloader/uboot-imx/drivers/net/phy

And I think that it is necessary to add a program file of the PHY that they use into this folder.

Is my understanding right?

Best Regards,
Yuuki

0 件の賞賛
返信

1,636件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

yes you are right, one can check ../drivers/net//mxc_fec.c

also one can look at appnote AN4173

Best regards

igor

0 件の賞賛
返信