About Spread Spectrum of PLL2 for DDR3L with i.MX6UL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About Spread Spectrum of PLL2 for DDR3L with i.MX6UL

跳至解决方案
1,468 次查看
yuuki
Senior Contributor II

Dear all,

We have a question about Spread Spectrum of PLL2 of i.MX6UL.

Only PLL2(SystemPLL) supports Spread Spectrum.

We want to use this Spread Spectrum for a peripheral.

However, this PLL2 is used for MMDC module.

When DDR3L is used, may this Spread Spectrum cause any trouble?

In this case should PLL4 be chosen for MMDC?

May I have advice?

Best Regards,

Yuuki

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
937 次查看
art
NXP Employee
NXP Employee

Please refer to the following community thread:

https://community.nxp.com/message/376642

It says that the DDR3 memories working at 528MHz can tolerate the spread spectrum operation with frequency deviation range of 5 - 6 MHz and frequency modulation rate of 20 - 60 kHz.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
938 次查看
art
NXP Employee
NXP Employee

Please refer to the following community thread:

https://community.nxp.com/message/376642

It says that the DDR3 memories working at 528MHz can tolerate the spread spectrum operation with frequency deviation range of 5 - 6 MHz and frequency modulation rate of 20 - 60 kHz.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
937 次查看
yuuki
Senior Contributor II

Dear all,

We want to apply Spread Spectrum for DDR3L to suppress the noise.

However, we must use PLL4 if Spread Spectrum adversely affects DDR3L.

May I have advice?

Best Regards,

Yuuki

0 项奖励
回复