About Spread Spectrum of PLL2 for DDR3L with i.MX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About Spread Spectrum of PLL2 for DDR3L with i.MX6UL

Jump to solution
1,316 Views
yuuki
Senior Contributor II

Dear all,

We have a question about Spread Spectrum of PLL2 of i.MX6UL.

Only PLL2(SystemPLL) supports Spread Spectrum.

We want to use this Spread Spectrum for a peripheral.

However, this PLL2 is used for MMDC module.

When DDR3L is used, may this Spread Spectrum cause any trouble?

In this case should PLL4 be chosen for MMDC?

May I have advice?

Best Regards,

Yuuki

Labels (1)
0 Kudos
Reply
1 Solution
785 Views
art
NXP Employee
NXP Employee

Please refer to the following community thread:

https://community.nxp.com/message/376642

It says that the DDR3 memories working at 528MHz can tolerate the spread spectrum operation with frequency deviation range of 5 - 6 MHz and frequency modulation rate of 20 - 60 kHz.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
786 Views
art
NXP Employee
NXP Employee

Please refer to the following community thread:

https://community.nxp.com/message/376642

It says that the DDR3 memories working at 528MHz can tolerate the spread spectrum operation with frequency deviation range of 5 - 6 MHz and frequency modulation rate of 20 - 60 kHz.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
785 Views
yuuki
Senior Contributor II

Dear all,

We want to apply Spread Spectrum for DDR3L to suppress the noise.

However, we must use PLL4 if Spread Spectrum adversely affects DDR3L.

May I have advice?

Best Regards,

Yuuki

0 Kudos
Reply