About QSPI for FPGA in i.MX6SoloX.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About QSPI for FPGA in i.MX6SoloX.

跳至解决方案
825 次查看
keitanagashima
Senior Contributor I

Dear All,

Hello. Now, my customer is considering to use the QSPI for FPGA connection.

[Q1]

Is it possible to use the QSPI for FPGA?

And, Is a QSPI driver prepared for FPGA?

[Q2]

When transferring the data using DMA, Is it possible to send the data without becoming Buffer Full of FIFO?

BSP:L3.14.28_1.0.0

Best Regards,

Keita

标签 (2)
0 项奖励
回复
1 解答
706 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

>[Q1]Is it possible to use the QSPI for FPGA?

yes.

>And, Is a QSPI driver prepared for FPGA?

no

>[Q2]When transferring the data using DMA, Is it possible to send

>the data without becoming Buffer Full of FIFO?

yes, behavior depends on QuadSPIx_RBCT[WMRK] setting

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
707 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

>[Q1]Is it possible to use the QSPI for FPGA?

yes.

>And, Is a QSPI driver prepared for FPGA?

no

>[Q2]When transferring the data using DMA, Is it possible to send

>the data without becoming Buffer Full of FIFO?

yes, behavior depends on QuadSPIx_RBCT[WMRK] setting

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复