About QSPI for FPGA in i.MX6SoloX.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About QSPI for FPGA in i.MX6SoloX.

Jump to solution
569 Views
keitanagashima
Senior Contributor I

Dear All,

Hello. Now, my customer is considering to use the QSPI for FPGA connection.

[Q1]

Is it possible to use the QSPI for FPGA?

And, Is a QSPI driver prepared for FPGA?

[Q2]

When transferring the data using DMA, Is it possible to send the data without becoming Buffer Full of FIFO?

BSP:L3.14.28_1.0.0

Best Regards,

Keita

Labels (2)
0 Kudos
1 Solution
450 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

>[Q1]Is it possible to use the QSPI for FPGA?

yes.

>And, Is a QSPI driver prepared for FPGA?

no

>[Q2]When transferring the data using DMA, Is it possible to send

>the data without becoming Buffer Full of FIFO?

yes, behavior depends on QuadSPIx_RBCT[WMRK] setting

Best regards

igor
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
451 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

>[Q1]Is it possible to use the QSPI for FPGA?

yes.

>And, Is a QSPI driver prepared for FPGA?

no

>[Q2]When transferring the data using DMA, Is it possible to send

>the data without becoming Buffer Full of FIFO?

yes, behavior depends on QuadSPIx_RBCT[WMRK] setting

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos