About LPDDR3 Initialization

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About LPDDR3 Initialization

1,932 次查看
goto11
Contributor III

Hello,Community

I connected imx7d and LPDDR3.
I want to set registers based on the Initialization Sequence of LPDDR3.
Is there any program code or program guide that can be used as a reference?

best regards

Goto

标签 (1)
0 项奖励
回复
2 回复数

1,827 次查看
igorpadykov
NXP Employee
NXP Employee

Hi goto11

one can look at Register Programming Aid:

i.MX7D DRAM Register Programming Aid 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,827 次查看
goto11
Contributor III

Hi igorpadykov

I checked Register Programming Aid.

I have a question about ”MX7D_LPDDR3_register_programming_aid_v1_4.xlsx” sheet “DStream .ds file”.
Should I write data to addresses in order from the top as shown below?
Is there a place where I need to wait or write dummy data?

memory set 0x ...

best regards

Goto

0 项奖励
回复