About GC7000L

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About GC7000L

1,963 Views
geyang
Contributor I

Hello NXP:

                  The device information is obtained through the clGetDeviceInfo () API as follows: 

Device Name: Vivante OpenCL Device GC7000L.6214.0000
Parallel compute units: 4
maxWorkItemPerGroup: 1024
maxGlobalMemSize: 256(MB)
maxConstantBufferSize: 64(KB)
maxLocalMemSize: 32(KB)

                  But,The “i.MX Graphics Users Guide GC7000L”datesheet about hardware information:

GPGPU cores  1

Shader cores   1

PE           16

so,Which should this relate to primarily

0 Kudos
Reply
2 Replies

1,802 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi,

The clGetDeviceInfo is primary.

0 Kudos
Reply

1,802 Views
geyang
Contributor I

How much PEs in GC7000L

0 Kudos
Reply