About EIM burst length in i.MX6SL.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About EIM burst length in i.MX6SL.

ソリューションへジャンプ
712件の閲覧回数
keitanagashima
Senior Contributor I

Dear All,

Hello.

First, refer to Table 20-6. AXI Burst Cycles Supported in IMX6SLRM(Rev.2).

It looks support only 16 word.

Next, refer to "BL" bits of 20.9.1 Chip Select n General Configuration Register 1 (EIM_CSnGCR1) in IMX6SLRM(Rev.2).

The description looks 32 words setting can be set.

Why did look the difference?

Best Regards,

Keita

ラベル(1)
0 件の賞賛
返信
1 解決策
650件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

you are right there is difference, because EIM and AXI bus

IP modules were developed independently and before i.MX6SL design.

These IP blocks are used in many processors.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
651件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

you are right there is difference, because EIM and AXI bus

IP modules were developed independently and before i.MX6SL design.

These IP blocks are used in many processors.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信