About EIM burst length in i.MX6SL.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About EIM burst length in i.MX6SL.

Jump to solution
583 Views
keitanagashima
Senior Contributor I

Dear All,

Hello.

First, refer to Table 20-6. AXI Burst Cycles Supported in IMX6SLRM(Rev.2).

It looks support only 16 word.

Next, refer to "BL" bits of 20.9.1 Chip Select n General Configuration Register 1 (EIM_CSnGCR1) in IMX6SLRM(Rev.2).

The description looks 32 words setting can be set.

Why did look the difference?

Best Regards,

Keita

Labels (1)
0 Kudos
Reply
1 Solution
521 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

you are right there is difference, because EIM and AXI bus

IP modules were developed independently and before i.MX6SL design.

These IP blocks are used in many processors.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
522 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

you are right there is difference, because EIM and AXI bus

IP modules were developed independently and before i.MX6SL design.

These IP blocks are used in many processors.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply