About Dual Display setting on MCIMX6Q-SDP + MCIMX-LVDS1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About Dual Display setting on MCIMX6Q-SDP + MCIMX-LVDS1

2,620件の閲覧回数
keitanagashima
Senior Contributor I

Dear All,

Hello. I have a question about Dual Display setting on MCIMX6Q-SDP + MCIMX-LVDS1.

I'd like to use the dual output to LVDS in L3.14.28_1.0.0.

- Output1 : LVDS on MCIMX6Q-SDP

- Output2 : MCIMX-LVDS (Connected to MCIMX6Q-SDP)

Could you tell me the way of above dual output for LVDS?

(I confirmed the FSL's document (Release note, User's guide). But, I couldn't find the setting method.)

Best Regards,

Keita

ラベル(3)
0 件の賞賛
返信
8 返答(返信)

2,274件の閲覧回数
art
NXP Employee
NXP Employee

Also, please refer to the following thread:

https://community.freescale.com/message/499774#499774

for the details on using dual LVDS on the i.MX6Q-SDP platform.


Have a great day,
Artur

0 件の賞賛
返信

2,274件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Keita,

Here do you want to use the two LVDS separate mode or dual mode?
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,274件の閲覧回数
keitanagashima
Senior Contributor I

Hi Dan,

We want to use the separate mode (display different contents on the different displays).

Best Regards,

Keita

0 件の賞賛
返信

2,274件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

It is already different display.

That is why I provide gstreamer command to do playback.

For dual or separate mode, it is application now in 3.10 and later.

0 件の賞賛
返信

2,274件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

setenv displayinfo 'video=mxcfb0:dev=ldb,bpp=24,if=RGB666  video=mxcfb1:dev=ldb,bpp=24,if=RGB666 video=mxcfb2:dev=none video=mxcfb3:dev=none'
setenv mmcargs 'setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot} ${displayinfo}'

Gstreamer playback to secondary display:

gst-launch-1.0 playbin uri=file:///media/AVC-1080P-9M_ToS.mkv video-sink="imxv4l2sink device=/dev/video18 disp-width=1920 disp-height=1080"

0 件の賞賛
返信

2,274件の閲覧回数
keitanagashima
Senior Contributor I

Hi Biyong,

SABRE-SDP could output to the dual LVDS Display by your command.

Thank you.

But, when I tried to video play on the secondary display, primary GUI display became strange.

(Video play on secondary display was no problem.)

Display.JPG

Do you know why is the phenomenon happened?

Best Regards,

Keita

0 件の賞賛
返信

2,273件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

if you just want to dual same UI on the LVDS0 and LVDS1. And it is the SDP board.

Use the prebuild binary image. Only change the device tree.

Modify the device tree and add  dual-mode; at line 817.

The attached imx6q-sabresd-dul.dtb is what I have tried working fine with  MCIMX6Q-SDP + MCIMX-LVDS1, 3.14.28_1.0.0_ga.

815 &ldb {

816         status = "okay";

817         dual-mode;

818         lvds-channel@0 {

819                 fsl,data-mapping = "spwg";

820                 fsl,data-width = <18>;

821                 status = "okay";

822

823                 display-timings {

824                         native-mode = <&timing0>;

825                         timing0: hsd100pxn1 {

826                                 clock-frequency = <65000000>;

827                                 hactive = <1024>;

imx6qdl-sabresd.dtsi

0 件の賞賛
返信

2,273件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

It is an application issue now.  

You could try the gstreamer to play back. 

0 件の賞賛
返信