About 2G LPDDR RAM test

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About 2G LPDDR RAM test

2,573件の閲覧回数
t2865k5
Contributor I

Dear NXP,

HW: imx8mpluse platform

You can refer the MX8M_Plus_MicronLPDDR4_2G_RAM.xlsx . The DDR calibratiob test is OK.(1500MHz)

I want to do a DDR reduction clock test. About "Clock Cycle Freq (MHz)3 " item,

I select 1400MHz/1300/MHz/1200MHZ to do DDR calibration test .

test result : fail.

 

May you provide me with 3 clock setting of frequency options below 1500 Mhz?

I hope it can pass the DDR calibration test.

t2865k5_0-1629266427308.png

 

0 件の賞賛
返信
1 返信

2,567件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi @t2865k5,

 

The RPA provides the DRAM_PLL_FDIV_CTL0 register (0x30360054) setting for 1500Mhz (0xFA080). For frequencies other than 1500Mhz, it is up to the user to create the appropriate register setting for the desired frequency. Formula is DDR_freq = [(24MHz x pll_main_div)/(pll_pre_div x 2^pll_post_div)] x 2

 

Hope this helps you.

Regards,

Israel.

0 件の賞賛
返信