About 2D / 3D graphics using i.mx8x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About 2D / 3D graphics using i.mx8x

1,428件の閲覧回数
YoshihisaSaitou
Contributor I

Dear Team,

Device: i.MX8QuadXPlus 

OS: Linux 4.9.88

Board:i.mx8QuadXPlus MEK

I use i.mx8x to evaluate graphics. So, there is one problem. I want to synchronize the drawing completion with Vsync of the display.(e.g. tearing)  I heard that this can not be done, but is it true?

If it can not be synchronized, I want to draw 60 fps. Is there a way to do it? I do not want to use eglSwapInterval ().

Best regards,

Yoshihisa Saito

0 件の賞賛
返信
1 返信

1,343件の閲覧回数
b36401
NXP Employee
NXP Employee

You can check if Vsync signal is on using GPIO loopback (with setting SION bit).

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信