AWS shadow ENET

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AWS shadow ENET

1,250 Views
Diwakar
Contributor I

Hi,

 I am using MIIMXRT 1170 EVK board  and working on AWS ENET Device shadow example. I am publishing the real time data on AWS IoT core in a loop. But This code is unexpectedly stops. I am getting the exact issue. 

So please try to solve my issue .  

0 Kudos
Reply
1 Reply

1,244 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Diwakar ,

   Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.

  Do you test the RT1170 SDK code directly for the aws shadow?

\SDK_2_10_1_MIMXRT1170-EVK\boards\evkmimxrt1170\aws_examples\shadow_enet\cm7

  You also need to check your network, make sure the connection and network is OK.

  If you directly test the SDK code, you can use your own AWS shadow, whether it works, do you also test it with the MQTTfx, whether it can also get the data?

  BTW, I have a post about the AWS, you can check it whether it is useful to you:

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/RT-cloud-testing-for-AWS-cloud-remote-control/ta...

From Jan.1th to Jan 3th is the Chinese New Year's Day, so, if you have any updated information, I will reply you after the holiday.
Thanks a lot for your understanding.

Best Regards,

Kerry

 

0 Kudos
Reply