AR8031 Spice model or S-Parameters

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AR8031 Spice model or S-Parameters

1,332 Views
anishmylari
Contributor I

Hai,

We arka-ims are working on Infotainment system using IMX6.

we are using AR8031 in our design for which we require the Spice model/S- Parameters for the analysis.

Can you please provide ?

Thanks

ANISH

0 Kudos
Reply
1 Reply

1,155 Views
igorpadykov
NXP Employee
NXP Employee

Hi ANISH

usually spice models are provided by chip  vendors, so it may be recommended to

apply directly to its tech support Contact Information | Qualcomm

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply