AIGLX error: drmOpenOnce failed (Operation not permitted)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AIGLX error: drmOpenOnce failed (Operation not permitted)

2,270 Views
prathameshghane
Fresh Out Contributor

Hi,

 

I am trying to run Xorg server on imx6 SABRE-AI. I was able to build vivante
module using LTIB. I put it in the file system, and am
now able to load vivante_drv.so through display.conf settings.Just to confirm
everything is ok, pasting brief log:

 

[    59.508]drmOpenDevice: node name is /dev/dri/card0

 

[    59.509]drmOpenByBusid: Searching for BusID platform:Vivante GCCore

[    59.509]drmOpenDevice: node name is /dev/dri/card0

[    59.509]drmOpenDevice: open result is 11, (OK)

[    59.509]drmOpenByBusid: drmOpenMinor returns 11

[    59.509]drmOpenByBusid: Interface 1.4 failed, trying 1.1

[    59.509]drmOpenByBusid: drmGetBusid reports platform:Vivante GCCore:00

 

Vivante driver loads a few more
modules (like fbdev,exa,fbdevhw etc), and I am getting some errors related to
AIGLX. Briefly, the message is something like this:

 

 

[    59.514]drmOpenDevice: open result is -1, (No such device)

[    59.514]drmOpenDevice: open result is -1, (No such device)

[    59.514]drmOpenDevice: Open failed

[    59.514]drmOpenByBusid: drmOpenMinor returns -19

[    59.514] (EE) AIGLX error: drmOpenOnce failed(Operation not permitted)

[    59.514] (EE) AIGLX: reverting to software rendering

[    59.514] (II) AIGLX: Trying DRI driver /usr/lib/arm-linux-gnueabi/dri/swrast_dri.so

[    59.646] (II)AIGLX: Loaded and initialized swrast

[    59.646] (II)GLX: Initialized DRISWRAST GL provider for screen 0

[    59.649] Fatal server error:

[    59.649] Driver failed PrepareAccess on a pinned pixmap.

 

Xorg versions for various drivers are as follows:


(II) Module ABI versions:

[    59.257] X.Org ANSI C Emulation: 0.4

[    59.257] X.Org Video Driver: 10.0

[    59.257] X.Org XInput driver : 12.3

[    59.257] X.Org Server Extension : 5.0

 

I want to know whether it is a problem related to just X-org version or something else is going wrong !!attaching a detailed log generated by startx for reference.

Thanks and regards,

Prathamesh

Original Attachment has been moved to: display.conf.zip

Original Attachment has been moved to: Xorg.0.log.zip

Labels (3)
Tags (4)
0 Kudos
Reply
1 Reply

1,843 Views
wallyyeh
Contributor V

I got the same message, did this work normal or what?

0 Kudos
Reply