AFE4490 interfacing with iMX6ULL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AFE4490 interfacing with iMX6ULL

1,358件の閲覧回数
mathew_k_t
Contributor II

Hi,

I'm trying to interface afe4490 with imx6ull through ecspi. I tested spi communication using spidev and I'm getting all signals when probed. But when interfacing afe4490 I'm not getting MISO signals. Do I need to do any configurations, if so how to configure it?

ラベル(3)
0 件の賞賛
返信
1 返信

1,245件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi mathew

suggest to ask vendor of that chip for linux driver or initialization sofwtare, as help

one can also look at

TI AFE4490 on labview - Page 2 - Discussion Forums - National Instruments 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信