ADV7180 to HDMI output blinking

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADV7180 to HDMI output blinking

1,338 次查看
racer
Contributor I

We are using ADV7180 as TV input, because our linux BSP code(L3.0.35_4.0.0)  has some conflicts with the "add-csi-deinterlace-capture.patch.zip"(download from De-interlace Capture Device) to support deinterlace input, I think the SDK may already fixed it.

the test command is:

>./mxc_v4l2_tvin.out -ow 720 -oh 480 -f YUYV

The display output is HDMI@1080p60

The output video is keeping blinking, the video clip can be find in attach, where the problem is?  on input video driver or output framebuffer setting?

0 项奖励
回复
0 回复数