A probability of USB hub failure when a 3.0 udisk was inserted on custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A probability of USB hub failure when a 3.0 udisk was inserted on custom board

916 Views
zhengguang_yang
Contributor II
When the system is booted with a 3.0 udisk was inserted on my board, there will be a probability of USB hub failure. When this happens, all USB interfaces from HUB can't be used.
Normal:
# lsusb
Bus 001 Device 005: ID 0951:1666
Bus 001 Device 002: ID 0424:2517
Bus 001 Device 001: ID 1d6b:0002
Abnormal:
# lsusb
Bus 001 Device 002: ID 0424:2517
Bus 001 Device 001: ID 1d6b:0002
SW version as follows:
BSP version :Yocto 2.1 
Kernel version: 4.1.15
But there is no such phenomenon on Yocto 1.8(Kernel version:3.14.52).
Labels (1)
0 Kudos
Reply
1 Reply

839 Views
igorpadykov
NXP Employee
NXP Employee

Hi

what bsp used in the case, one can try with nxp official Demo Images from link

i.MX Software|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply