8MQ for DDR4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

8MQ for DDR4

1,807 Views
haochengdong
Contributor II

Why does the 8MQ DDR4 reference design use T PCB routing topology for a 2-rank system? Is it because the addressable range of a single DRAM_nCS is too small? Can it be designed as T PCB routing topology for a 1-rank system. Only one DRAM_nCS0 is used.

2 Replies

1,723 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Haochengdong Haochengdong,

A 2-rank system is implemented on the EVK and recommended as it may provide better performance and it allows to use the T topology to mirror the chips and make it easier to design, although a single rank design is also possible, as Mrudang mentions.

 

However, in general terms I would recommend that you follow the recommendations for DDR design on the i.MX8QM Hardware Design Guide (link below, please note that you may need to login to download this document) unless you are very confident in DDR4 design as routing DDR4 memories can be challenging.

https://www.nxp.com/webapp/Download?colCode=IMX8MDQLQHDG

I hope this helps!

Regards,

1,723 Views
mrudangshelat1
Senior Contributor II

Hi,

It is possible to design 8MQ DDR4 PCB routing topology for a 1-rank system as long as you are able to get your requires memory density. The reference design has used 2 rank system to achieve their memory density.

Mrudang