8MMINID4-EVK Power On booting & shutdown modification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

8MMINID4-EVK Power On booting & shutdown modification

2,463 Views
nikunj_mehta
Contributor II

Hi Team,

We have Development Boards & Kits - ARM 8MMINID4-EVK , we are using Android image . 

Our requirement is when user give reboot -p  / Shutdown , Device should not going in shutdown mode its start rebooting only ( if board have power ) . so use case is if power off then and then device shutdown other wise it always in on condition . 

Tags (1)
0 Kudos
Reply
2 Replies

2,385 Views
Yuri
NXP Employee
NXP Employee

[email protected] 

Hello,

    i.MX validation boards and NXP sponsored third­party boards have all been designed
to remove power (Voltage source) to all components on the board in the event of
a processor reset. This is provided in order to avoid iMX SOC boot issues, when
power is not removed.
  Such external components as SD Card/socket (if the reset pin is not used to
remove power to the SD Card), QSPI, NOR, LPDDR2/3 memory have internal state machines,
which can be in non-proper (non-reset) state for boot.
   The best solution here is providing Power On Reset if system should be reboot.

Regards,

Yuri.

0 Kudos
Reply

2,385 Views
nikunj_mehta
Contributor II

Yes , But i am asking about change in shutdown mode , like even if i am giving shutdown ( reboot -p) command then also my device work as simply reset / reboot configuration .

i think we have to modify power driver but i am not sure how to modify it .

0 Kudos
Reply