8M Quad support to deep learning frameworks?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

8M Quad support to deep learning frameworks?

1,896件の閲覧回数
roger_kupari
Contributor I

Hi,

I have been thinking about this question for a while: is the 8M quad that industrial version capable to run frameworks like Tensorflow or/and Caffe and processing the moving object recognition? Of course the image processing includes in that question.

The framework will be driven under operating system, Linux.

I think its capable to that, but there would be some problems on timing the process.

I have planned to use 5 MP camera based on OV5640 chip and some small HD-scale colored TFT-screen. Both maybe connected by the MIPI bus.

The timing between input and output (camera -> image processing -> recognition -> result on the screen with the picture).

I expect like realtime results on output (min 30 fps), so the time to output per picture can be something like 30 milliseconds at least.

Is the i.MX 8M Quad or even QuadLite capable to run process with these limits?

Or is it better to just wait the i.MX 8 launch?

Thanks in advance

Br. Roger

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,701件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Roger,

The i.MX8M is capable of running Tensorflow or/and Caffe and support deep learning frameworks.

Regards

0 件の賞賛
返信

1,701件の閲覧回数
PramodKumar
Contributor IV

Tensorflow or Tensorflowlite is better for moving object detection in i.MX8M

0 件の賞賛
返信