8G eMMC change to 16G eMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

8G eMMC change to 16G eMMC

Jump to solution
4,263 Views
wanglee
Contributor III

          我们用iMX6Q芯片开发了一套板卡。能够正常使用。启动方式是eMMC,原来用的eMMC是东芝的的THGBM5G6A2JBAIR, 后来应客户的需求更换为SDIN5C2-16G,更换之后无法正常下载程序,会卡在如下图的地方,请问这个是焊接问题吗?iMX6Q支持16G的eMMC吗?如果支持,需要修改uboot?有没有相关的技术文档?

  C6U8PYB7WD`7{H}U~6GQ1RY.png

Labels (1)
0 Kudos
Reply
1 Solution
3,949 Views
igorpadykov
NXP Employee
NXP Employee

Hi wang

iMX6Q can support 16G eMMC, however there may be signal integrity

issues as for example below

https://community.freescale.com/thread/332110

In such case it is necessary to rebuild mfg tools firmware.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
3,949 Views
mikeliu
Contributor I

https://community.freescale.com/thread/332110

这个地址失效了,我现在也遇到同样的问题了

0 Kudos
Reply
3,950 Views
igorpadykov
NXP Employee
NXP Employee

Hi wang

iMX6Q can support 16G eMMC, however there may be signal integrity

issues as for example below

https://community.freescale.com/thread/332110

In such case it is necessary to rebuild mfg tools firmware.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------