3Dmark test on iMX6 PLEASE!!!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

3Dmark test on iMX6 PLEASE!!!

2,521件の閲覧回数
edelm
Contributor III

Hello, has anyone tried 3Dmark test on i.MX6q board?

At some reason i cannot get more than 6fps... The libEGL and libGLESv1 and v2 loaded ok, but still no luck to get it working.

ラベル(5)
タグ(5)
0 件の賞賛
返信
3 返答(返信)

2,299件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

which BSP of Android did you try?, and which test from 3DMark did you do?

0 件の賞賛
返信

2,299件の閲覧回数
edelm
Contributor III

I almost gave up..

I use Andorid 4.2.2 latest release, from boundary devices.

the 3Dmart is the one from Play Store. I guess it's the latest too.

Thanks!

0 件の賞賛
返信

2,299件の閲覧回数
edelm
Contributor III

Hello, anyone?

It's not hard, just load the test from the Play Store and let it run once.

0 件の賞賛
返信