32bit rootfs on 64bit kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

32bit rootfs on 64bit kernel

2,230 Views
sivasubramanian
Contributor I

Hi,

AFAIK there is multilib support available on iMX8 to build 32bit libraries on rootfs. But is there any option to have full 32bit rootfs on 64bit kernel (boot & modules)?

Regards,

Sivasubramanian

Tags (3)
0 Kudos
Reply
1 Reply

2,046 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sivasubramanian

one can check AN12212 Software Solutions for Migration Guide from Aarch32 to Aarch64

https://www.nxp.com/docs/en/application-note/AN12212.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply