2MIC audio with android things

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2MIC audio with android things

1,301 Views
Felix_Zhang
Contributor II

The solution is based on android things to realize google assistant & cast, need to connect 2MIC signal & 2 AEC signal to MPU. Is the connection in the sch right? 

1.Is it right to use SAI3 for  4 channel ADC signal input?

2.Is it right to use SAI1 for  speaker signal output?

3.Does PICO-PI-IMX7 support TDM format?

xx.png

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

1,197 Views
igorpadykov
NXP Employee
NXP Employee

Hi felix

1. yes

2. yes

3. I am not familiar with PICO-PI-IMX7 board, but its processor SAI

    supports TDM format. Regarding software support, it can be posted on vendor

    support: Support - TechNexion 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply